Accommodations near Braunau
Accommodations near Braunau
Lodging | Website | Distance to seminar location |
---|---|---|
Sovea Hotel Braunau | 0.1 km | |
Schüdlbauers Hotel | 1.5 km | |
Hotel Gann | 1.9 km | |
Das alte Gefängnis (the old prison) | 1.9 km | |
Schlosstaverne restaurant | 2.3 km | |
Old town hotel Mayrbräu | 2.4 km | |
Hotel am Theaterpark | 2.4 km | |
Pension Göttler | 4.9 km | |
Pension Moosbräu | 5.1 km | |
Motel Inn | 5.3 km |
Interesting information about the region
Interesting information about the region
The Innviertel region is located in the northwest part of Upper Austria and includes the districts Braunau am Inn, Ried im Innkreis and Schärding. Unlike the rest of Upper Austria, this region was mostly part of Bavaria up until 1779 (Treaty of Teschen). Referring to this region as the Innviertel is something that is relatively new (before it was commonly called Innbaiern). The new term was created by the Austrian government after annexation in 1779, which also divided the territory into four quartersSee also: en.wikipedia.org/wiki/Innviertel. More information about this is available here:
Event address and organizers
Event address and organizers
The B&R summer workshop takes place annually at the HTBLA Braunau.
Event location | Organizer |
---|---|
HTLBA Braunau/Inn Osternbergerstrasse 55 5280 Braunau Austria | B&R Industrial Automation GmbH B&R Strasse 1 5142 Eggelsberg +43(0)7748/6586-0 |