In terms of footprint, Optima's innovative solution has a clear advantage over systems that use conventional technology for product grouping. "With a conventional construction using screws, the grouping function requires a machine frame with two fields, each 220 centimeters long," explains Dreschner. "The ACOPOStrak solution, however, adds just 80 centimeters to the overall length of the system, so it's almost four meters shorter than before."
Nevertheless, it achieves a higher throughput than its conventional counterpart: The food retailer produces and packages 720 capsules in 72 cartons every minute. There are a total of 80 shuttles in circulation. They are distributed over two separate, stacked oval tracks, each 7.2 meters long.
One reason for the division into two tracks was the required spacing between the products of under 50 mm, although the shuttles themselves are already 50 mm wide. The track ovals and the product carriers are therefore designed in such a way that the grippers of the upper oval and those of the lower oval come to rest alternately at the same level. At this level, the product carriers are each only about 40 mm wide, so the required product spacing of under 50 mm can be achieved.